cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN32F0 and STEVAL-SPINS3201 Problem

ekocakaya
Associate

Hello friends,

I made a custom STSPIN32F0 board , copy all sames STEVAL-SPINS3201 except STM32F103 side ,

We upload default software from motor library and system works well in EVM SPINS3201 but when we upload same software to our boards , there is no movements,

When we checks registers, system stuck in FAULT_OVER or IDLE mode, system not turn to RUN mode

What is the problem can be? we checked all board , there is no difference with EVM board

Any idea?

1 REPLY 1
cedric h1
Associate III

Hello,

Do you have an UART connection with your board ? If yes are you able to connect with motorcontrol workbench ?

Did you check that your code reach the while loop in the main.c ?

Regards

Cedric

If you agree with my answer, please accept it by clicking on 'Accept as solution'."