cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL PCC009V2 & SPINFamily Evaluation Tool

Cooke.Ernest
Associate II
Posted on April 04, 2017 at 17:31

Hi,

I am trying to use the STEVAL-PCC009V2 & EVAL6470H boards using the SPIN

Family Evaluation Tool (Version 3.2)

However when I try to connect to the board I get the following error:

0690X00000606d4QAA.png

I have managed to locate the below hex file at the following location:

C:\Program Files (x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Firmware

0690X00000606dnQAA.png

I have tried to download the hex file below onto the board using Keil uVision but I am getting the following error in the Build Output.

0690X00000606hFQAQ.png

It should be noted that I was able get older versions of the SPINFamily Evaluation Tool to work.

If anyone has any solutions to this problem or has a link to Version 3 of the Evaluation Tool I would greatly appreciate it.

Kind Regards,

Ernest Cooke

#dspin #pcc009v2-eval6470h-spinfamily #dspin-gui #powerstep01 #keil-uvision
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
dungeonlords789
Senior III

BUG at SPINFamily Evaluation Tool (STSW-SPIN002)

There is a bug when I use ihm03a1 with SPINFamily Evaluation Tool. I am creating new settings for my motor, select Voltage mode, and resistance > 2 Ohm. So SPINFamily Evaluation Tool throw fatal exception.

dungeonlords789
Senior III

My motor has 5 Ohms resistance. When I try to set 5 Ohms at SPINFamily tool for ihm03a1 - application crash! Is it a bug of application?

Thanks for your instruction. It works for me !