2023-12-05 1:18 PM
When testing discovery kit. With Demo 1 binary file FW of the STSW-L9961BMS. Tera Term serial monitor outputs random characters. Using Speed 9600, Data 8 bit, Parity none, Stop bit 1 bit. Tried different computer. Tried different settings. Same result. Display nothing like VT100 User Interface.
2023-12-14 8:21 AM - edited 2023-12-14 8:23 AM
Hello,
sorry for the delayed answer.
Did you try to set UART baud rate at 115200 ?
It should be the right one.
Regards.
Ignazio
2023-12-15 1:40 AM
Ciao KWarr.1,
it seems that the problem is due to a wrong UART baudrate setting.
Please, cross check the suggested values, so as reported within the source code and the snapshot.
Best Regards,
Nicola.
2023-12-15 3:01 AM
When I select 115200 baudrate, I get a flash error massage NO DEVICE FOUND from Tera Term VT.
2023-12-18 7:51 AM
Dear User,
getting that kind of (error) message means that the communication with the system is well established, but the device is not powered: please, check that the L99615C has a proper supply (i. e., greater than 14V, even 20V).
Best Regards.
Nicola.