2024-02-26 12:51 AM
I hope all is well with you,
As mentioned in a separate subject, I use my solar panel connected to the STEVAL-ISV020V1 to charge my LiPo battery. I wonder if you can help me figure out the total resistance of the STEVAL-ISV020V1 board when it operates in my project. Attached below is the connection
Thank you and hoping to hear from you soon!
Best regards.
2024-02-26 2:22 AM
In addition, the output voltage of my PV is around 4V which means that it meets the required input PV voltage to operate the STEVAL-ISV020V1 board which must range from 2.6V to 9V. My concern is when I connect the output of my solar panel to the STEVAL-ISV020V1 board (same connection as attached),
why does the voltage measured suddenly decreased below 1V?
Also since what happens if the battery is already below 3.7V, will the STEVAL-ISV020V1 board to which I connect my 4V PV still charge the battery?
2024-02-26 2:55 AM
Sorry to have so many queries. This is related to my last question, what if my battery measures 7 V which is beyond the EOC threshold 4.2 V, how will the STEVAL-ISV020V1 board respond to this? Will it let the battery drain until it reaches the range 3.7 V to 4.2 V to operate the UVP and EOC correctly?