cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ISB68WA - Formula for deriving capacitor and inductance values

HWong.6
Associate II

Hi.

We are students working on a hardware project. We are designing based on the STEVAL-ISB68WA design and would like to know the derivations which could aid in our design(the formula for calculating the capacitor and resistance values).

Is there anywhere that we can find such information available? Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @HWong.6​, to the community!

there aren't a lot of resistors in the STEVAL-ISB68WA so I'm guessing you confused it with the inductor coil?

The coil is an important and central part of the Qi receiver, so best would be to start reading AN5535 - Coil selection tool guide for STWLC68GUI.

The datasheet of the STWLC68, section 6.2., could also be very helpful, although it indicates right at the beginning that:

The design of the receiving series resonant circuit, namely the receiving coil (Ls), the resonant capacitor (Cs) and the detection capacitor (Cd), is out of the scope of this document. In principle the resonant capacitor and the detection capacitor are easily calculated via simple equations involving standardized or customized resonance frequencies.

...and references e.g. to documents like:

  • The Qi Wireless Power Transfer System; Power Class 0 Specification; Version 1.2.2
  • PMA Inductive Wireless Power Transfer Receiver Specification - System Release 1

from e.g. the Wireless Power Consortium.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Cristiana SCARAMEL
ST Employee

Hello @HWong.6​ and welcome to the ST Comunity.

since your question is about a wireless charger application, I moved your thread from the topic Motor Control Hardware to the dedicated ones.

If you feel a post has answered your question, please click "Accept as Solution"
Peter BENSCH
ST Employee

Welcome, @HWong.6​, to the community!

there aren't a lot of resistors in the STEVAL-ISB68WA so I'm guessing you confused it with the inductor coil?

The coil is an important and central part of the Qi receiver, so best would be to start reading AN5535 - Coil selection tool guide for STWLC68GUI.

The datasheet of the STWLC68, section 6.2., could also be very helpful, although it indicates right at the beginning that:

The design of the receiving series resonant circuit, namely the receiving coil (Ls), the resonant capacitor (Cs) and the detection capacitor (Cd), is out of the scope of this document. In principle the resonant capacitor and the detection capacitor are easily calculated via simple equations involving standardized or customized resonance frequencies.

...and references e.g. to documents like:

  • The Qi Wireless Power Transfer System; Power Class 0 Specification; Version 1.2.2
  • PMA Inductive Wireless Power Transfer Receiver Specification - System Release 1

from e.g. the Wireless Power Consortium.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.