2019-09-25 03:42 AM
Hi,
I'm facing some really weird problem with STC3100. After powerup I try to enable operating mode by writing 0x10 value (GG_RUN bit) to register REG_MODE at address 0x00. I2C address is 0x70 as default. STC3100 sends ACK for I2C address, also for register address, but NEVER for data byte, i.e. I never get last ACK. I tried to change clock frequency 10KHz/100KHz/400Khz without any success. How that can be?
Same magnified:
2021-06-29 08:56 AM
did you ever find out what the issue was ?
2021-06-29 09:03 AM
Hello!
Unfortunately no. I have created this thread with a hope to get some support from ST, but didn't get any answer. I replaced STC3100 with STC3115 in my device.
STC3115 works properly without any issues at all.
2021-06-29 09:23 AM
OK, I am seeing the same thing (lucky me)
Thanks for the recommendation - I will take a look.
2021-06-29 01:01 PM
Hello,
I believe that I have tracked the problem down to the part being in under-voltage lock-out
When the power to the part is below the threshold of 2.7 volts - I can't write the registers.
Above a threshold - it works.
What I am seeing now is the part sees any short excursion below the threshold, and immediately goes into lock-out.
I will add an R-C filter for the power in the future.