cancel
Showing results for 
Search instead for 
Did you mean: 

start up motor with hall

jgil
Associate II
Posted on February 09, 2009 at 05:18

start up motor with hall

2 REPLIES 2
stello
Associate II
Posted on May 17, 2011 at 10:15

Hello ihsguru,

Encoder is a relative sensor it means that any movement respect to initial position can be monitored using this kind of sensor. On the contrary, FOC needs the absolute rotor position information and a pre-positioning step is thus necessary to synchronize the real angle and the SW angle.

On the contrary, Hall sensors provide you with an absolute rotor position information. It means you exactly know where the rotor is (except for a uncertainty of +/-30 electrical degrees at start-up) and you don't need thus to perform any pre-positioning steps.

Regards,

BilLino

jgil
Associate II
Posted on May 17, 2011 at 10:15

Hello

At sensored hall motor control why not align or ''ramp up'' on start up as ST7FMC?

Thank you