2021-05-11 4:30 AM
Hi,
I installed 25 of the ST1S41 on a PCB and tested them with different Bench Power Supply and a electronic load or motors on the output. Everything worked very well till I swapped the Bench supply for a lithium Battery. Once I connected the Battery the switching regulator chips literally exploded. Has someone a explanation for that behavior and/or a solution for the problem?
Another Test I want to do but have not so far is to connect a little circuit between battery and converter that ramps the voltage up slowly (maybe 10ms).
Additional Info:
For the PCB Layout I followed the recommendations in the datasheet closely (see attached circuits and layout). There is a 100u capacity at input side of each converter and a 47u cap on output. The enable pin of the chip was pulled low when the battery had been connected. I was able to reproduce the behavior with one isolated chip (with only the necessary components connected)
Help and elucidation is much appreciated,
Best regards,
Tobias Friebel
2023-06-23 7:11 AM
Interesting test, did you find the cause of the problem?
2023-06-23 12:52 PM
After a rough check of the layout, I could not find any noticeable errors.
I would be interested in the parameters of the bench supply and the lithium battery, i.e. voltage and internal resistance?