Skip to main content
TFrie.1
Visitor II
May 11, 2021
Question

ST1S41 step-down switching regulator destroys itself on low impedance power source

  • May 11, 2021
  • 2 replies
  • 1184 views

Hi,

I installed 25 of the ST1S41 on a PCB and tested them with different Bench Power Supply and a electronic load or motors on the output. Everything worked very well till I swapped the Bench supply for a lithium Battery. Once I connected the Battery the switching regulator chips literally exploded. Has someone a explanation for that behavior and/or a solution for the problem?

Another Test I want to do but have not so far is to connect a little circuit between battery and converter that ramps the voltage up slowly (maybe 10ms).

Additional Info:

For the PCB Layout I followed the recommendations in the datasheet closely (see attached circuits and layout). There is a 100u capacity at input side of each converter and a 47u cap on output. The enable pin of the chip was pulled low when the battery had been connected. I was able to reproduce the behavior with one isolated chip (with only the necessary components connected)

Help and elucidation is much appreciated,

Best regards,

Tobias Friebel

    This topic has been closed for replies.

    2 replies

    LCE
    Principal II
    June 23, 2023

    Interesting test, did you find the cause of the problem?

    Peter BENSCH
    ST Technical Moderator
    June 23, 2023

    After a rough check of the layout, I could not find any noticeable errors.
    I would be interested in the parameters of the bench supply and the lithium battery, i.e. voltage and internal resistance?

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.