cancel
Showing results for 
Search instead for 
Did you mean: 

ST1S14PHR power instability

lbug.1
Associate

I'm using ST1S14PHR like the attached schematic, but with an input between about 10V and 20V the output is instable and appears 2.8/3.2V ...sometimes after a few seconds the stable situation at 5V is reached.

After the ST1S there is a linear 3v3 regulator that with the instable input has an instable output.

Absorption at 24V is about 30mA.

What could be the problem?

thanks...

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0