2024-07-05 4:50 AM - last edited on 2024-07-05 5:14 AM by Peter BENSCH
Hi,
I am looking for a spice model for this mosfet (preferably one that runs stable in LTSpice).
Purpose is to do some simulations for a SMPS (detailed calculation during transients should be supported by the model).
I did not find in STB60NF06 - N-Channel 60V - 0.014Ohm - 60A - D2APK StripFET(TM) II POWER MOSFET - STMicroelectronics
(For some mosfets, it is available at this place).
Is a model for this mosfet available?
Herwig.
Solved! Go to Solution.
2024-07-05 5:21 AM
The AI says :
The STB60NF06 is a N-Channel 60V - 0.014 Ohm - 60A DPAK STripFET II MOSFET from STMicroelectronics. The spice model for this device is not explicitly provided in the search results. However, the device’s datasheet can be used to create a spice model.
Device Parameters
Note
The spice model for the STB60NF06 can be created using the device’s parameters and characteristics. However, the exact spice model is not provided in the search results.
2024-07-05 5:16 AM
Welcome @Herwig, to the community!
The MOSFET was launched in 2004, when spice models were still rarely available. I fear that no more models will be created for such an old device.
Regards
/Peter
2024-07-05 5:21 AM
The AI says :
The STB60NF06 is a N-Channel 60V - 0.014 Ohm - 60A DPAK STripFET II MOSFET from STMicroelectronics. The spice model for this device is not explicitly provided in the search results. However, the device’s datasheet can be used to create a spice model.
Device Parameters
Note
The spice model for the STB60NF06 can be created using the device’s parameters and characteristics. However, the exact spice model is not provided in the search results.
2024-07-05 5:40 AM
Ok.
Thanks for the feedback.