cancel
Showing results for 
Search instead for 
Did you mean: 

VN9E30F Channel deatils

KumarTP
Associate III

 

VN9E30FTR – 6-channel high-side driver with 24-bit SPI interface

Max. DC output current is internally limited to 35A for channels IOUT0, IOUT1, IOUT2, IOUT3, IOUT4, and IOUT5

  1. Whether this 35A limit is shared across all channels or applies individually to each channel.
  2. What is the maximum current for each channel
  3. Conditions applicable when switching the load per channel.
  4. Can we parallel 2 or 3 channels to get single output.
  5. If we are not using any channel cant it be disabled / floated ( Is SOCR used for Enabling / disabling the channel )
1 REPLY 1
Maxime_MARCHETTO
ST Employee

Hello @KumarTP,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.