2017-12-02 03:18 AM
I having traouble with the H-Bridge 'VNH5180A'. I tried to find the problem now for some days, but I wasn't able to find it.
The H-Bridge haven't the right output voltage.
At the Pins of the Bridge are these voltages. I measured them with an oscilloscope:
designation
Voltage before the resistors
Voltage at the pins of the H-Bridge
CS
0
0
CS_DIS
0
0
EN_A
5
5
IN_A
0
0
EN_B
5
5
IN_B
3,3
3,3
OUT A | Motor1
DutyCycle 50% | 8 kHz | 0-0,5V
DutyCycle 50% | 8 kHz | 0-0,5V
OUT B | Motor2
12
12
PWM
DutyCycle 50% | 8kHz | 3,3V
DutyCycle 50% | 8kHz | 0-3,3V
Vcc
12
12
Attached is a picture of my layout, of the datasheet from the H-Bridge and an Osziloscop picture of the H-Bridge output Out_A -Out_B.
Thanks for your help in advance.
#vnh5180 #h-bridge #h-bridge2018-01-08 02:42 AM
Hello
matthias.romfeld
,thanks for your question.
Please double check that load (also resistive) is connected to the output, this is a standard behavior when no load is connected to the output pin.
Please let us know.
Regards
Davide
2018-05-10 04:39 AM
Thanks for the answer. Sorry for my late reply. We have solved the Problem with your tip
Thanks!