Posted on January 08, 2018 at 13:03Hi Hans,We confirm that VNH5019 max current capability is 30A, since this is the min current limitation. On the other hands, managing such high power inside the chip, you have to take under consideration also the t...
Posted on January 08, 2018 at 11:42 Hello matthias.romfeld, thanks for your question. Please double check that load (also resistive) is connected to the output, this is a standard behavior when no load is connected to the output pin. Please ...
Posted on October 19, 2017 at 15:08Hello Brian,you can replace the VN7140AJTR with VN7040AJTR, VN7050AJTR, VN7020AJTR.They are fully pin to pin compatible, please have a look to the following page:http://www.st.com/en/automotive-analog-and-power/hi...
Posted on June 13, 2017 at 10:53Hi,could you please provide further info about the components used for the protection circuit?Have you already had a look at the Application Note UM1922?Best regards.Davide
Posted on March 15, 2017 at 12:51Hello, Vsense is the voltage on CS (Current Sense) pin. This pin acts as a current generator and a current proportional to the motor current is sourced from this pin. The voltage on the pin depends thus on the motor ...