2022-02-24 05:40 AM
3 Powersteps -> 3 steppingmotors for X, Y and Z axes, voltage mode.
Is there a way to switch cleanly between MOVE and RUN commands?
Currently, when I execute RUN command after MOVE movement, motors move too slowly. Although I change the speed (target - acceleration from 0 to 1200 RPM).
MOVE alone works fine, RUN curves without MOVE also clean.
Of course I wait for SMCMD_READY, and only then I send next command with SPI.
Solved! Go to Solution.
2022-02-28 11:09 PM
This was interface error . Problem solved
2022-02-28 11:09 PM
This was interface error . Problem solved
2022-02-28 11:46 PM
Thank you for letting us know!
However, you are also welcome to post more details about the temporary misbehaviour so that other users can avoid it. Thank you!