2025-06-27 5:45 AM - last edited on 2025-06-27 6:33 AM by Andrew Neil
Hi,
I have a question about the RUN command because there are different speed to MOVE command.
In RUN command the speed min its 0,015 Step/second , in MOVE command the max speed min it is 15.25 Step/Second.
I need run the motor at very low speed similar to RUN command but i need set the number of step.
Are there a solutions ?
Thank you.
Giorgio Tessari
2025-08-19 2:52 AM
Hi @GiorgioTex ,
if you want to run the motor with very low speed, I suggest either to use the step-clock driving mode (a signal with the desired frequency connected to STCK pin that triggers a single step movement) or to provide a MOVE command of 1 step with the desired period
Alessio