cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control Library maximum modulation index

peterdonchev
Senior
Posted on March 21, 2018 at 10:37

Hi,

I have question about maximum modulation index in motor control library. When it is 100% is there any danger at very low RPM high side driver's bootstrap capacitors to be completely discharged? Is there any mechanism which guarantee that low side of the half bridge will be switched on in predefined interval of time?

#modulation-index #motor-control-library
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0