cancel
Showing results for 
Search instead for 
Did you mean: 

low voltage BLDC drive? urgent

huaer2000
Associate II
Posted on August 03, 2004 at 10:40

low voltage BLDC drive? urgent

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
huaer2000
Associate II
Posted on May 17, 2011 at 10:17

Dear sir,

I want to use ST72141 to drive a bldc, the requirements are as follows:

open loop, speed 2000-20000rpm, voltage

I want to know If I can use ST72141 in this case?

Best Regards,

Mucinterest
gaetano
Associate II
Posted on May 17, 2011 at 10:17

Hello,

I would like to know if you are interested at the ST72141 specifically or the new ST7MC could be interesting for you as well. The new one offers several features and tools helping to speed up the apply.

If 10V (or less) is the motor supply voltage no problem for both the micro to run at your specifics.

The major issues depen on the inverter topology and not on the micro features.

In the same site you find some application notes related with low voltage applications when using these type of micros running BLDC motors.

Let me know for further info or help.

Best regards,

Gaetano