cancel
Showing results for 
Search instead for 
Did you mean: 

Can't get Practispin Going - Please Help....

kland
Associate II
Posted on August 10, 2004 at 14:33

Can't get Practispin Going - Please Help....

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
kland
Associate II
Posted on May 17, 2011 at 10:17

Hello,

I've got a EVAL6208PD board with Practispin ST7 based driver board.

Problem is I can't get the Practispin software to speak to the ST7 board over RS-232. The board has 5V (5.01V) coming from the 6208PD board and I get 5V on the processor and max232 chip. I adjusted R18 to 50% as the instructions call for.

All seems well except it won't communicate.

Is there some trick? I've tried two different known working cables on 3 different known working PC's.

Any ideas?

If anyone has a known working practispin and/or 6208PD board they would like to part with I'd be happy to purchase it/them.

Thanks,

Ken

kland
Associate II
Posted on May 17, 2011 at 10:17

Looks like a bad Max232 chip. With the logic analyzer I can see data going into the 232 level converter chip, but nothing going out to the mpu.

Joy, another month to get a replacement board? I ordered a handful of 232 replacement chips as well.

Let me know please if you know anything, or can expedite a replacement, or have a working board you would part with.

Thanks,

Ken

[ This message was edited by: KenLand on 05-08-2004 14:52 ]
kland
Associate II
Posted on May 17, 2011 at 10:17

Well, I replaced the 232 chip and no joy.

Is there any way to get support on this thing?

Thanks,

Ken