cancel
Showing results for 
Search instead for 
Did you mean: 

LDO29300P2MTR

saran
Associate II

We have implemented the following circuit. This matches the application circuit given in datasheet of LDO29300P2MTR.But it does not yield expected output. We need help!!IMG20250328160749.jpg

13 REPLIES 13
saran
Associate II

@Andrew Neil 

The chip gives expected output 12V but within a fraction of second , voltage drops to 0V.

saran
Associate II

@Andrew Neil 

@Peter BENSCH 

 

Thanks for the help. LD29300P2MTR will work on 2.5 V to 14V only. it will never work greater than 14V. We can use the MIC29302WU 

 

Thanks &Regards,

Saravanan G

Sorry, I had also overlooked this during a cursory glance at the data sheet: although the LD29300 can withstand an input voltage of up to 30V, it actually only works up to 14V. This can be found in the data sheet as footnote 1 under table 2:

Above 14 V the device is automatically in shutdown.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@Peter BENSCH wrote:

This can be found in the data sheet as footnote 1 under table 2:

Above 14 V the device is automatically in shutdown.


So it does!

@saran - here:

AndrewNeil_0-1743410407092.png

@saran - always important to understand that these "Absolute Maximum" ratings are not operating specs!