cancel
Showing results for 
Search instead for 
Did you mean: 

LDO29300P2MTR

saran
Associate III

We have implemented the following circuit. This matches the application circuit given in datasheet of LDO29300P2MTR.But it does not yield expected output. We need help!!IMG20250328160749.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
saran
Associate III

@Andrew Neil 

I have attached the images for your reference. Kindly let me know if I have made any mistakes

 

saran_0-1743219895566.png

WhatsApp Image 2025-03-29 at 9.11.29 AM.jpegWhatsApp Image 2025-03-29 at 9.23.29 AM.jpegWhatsApp Image 2025-03-29 at 9.27.10 AM.jpeg

View solution in original post

13 REPLIES 13
Andrew Neil
Super User

@saran wrote:

 it does not yield expected output. !!


So what output does it yield ?


@saran wrote:
AndrewNeil_0-1743160143634.png

What is the significance of the 5.41A there?

The LD29300 is only a 3A regulator ...

https://www.st.com/en/power-management/ld29300.html 

 


@saran wrote:

This matches the application circuit given in datasheet 


Not quite:

AndrewNeil_1-1743160439834.png

You've left the INH pin open.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
saran
Associate III

The IC takes an input voltage of 24V/5.4A , expected output is 12V BUT IT GIVES 0V . Also where should I connect the INH pin.

Peter BENSCH
ST Employee

+1

And for an output voltage of 12V that can be set within narrower limits, I would replace VR1 with 1k and connect an 8.2k resistor in series to VR1. The output voltage should then be adjustable between approx. 11.2V-12.6V.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@saran wrote:

The IC takes an input voltage of 24V/5.4A 


The IC takes an input voltage; the current is determined by the load.

 


@saran wrote:

expected output is 12V BUT IT GIVES 0V . .


The output depends on R1 - so what do you have that set to?

 


@saran wrote:

where should I connect the INH pin.


As the datasheet shows - connect it high for 'ON', or low for 'OFF':

AndrewNeil_0-1743162989485.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
saran
Associate III

@Andrew Neil

R1 value is 10Kohm ; R2 is 1Kohm

@saran Let me tell you what is meant by INH=H: simply connect INH (pin 1) to INPUT (pin 2) to switch the LD29300 on permanently. If you connect pin 1 to GND, you switch it off.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
saran
Associate III

@Peter BENSCH

I have shorted pin 1 and pin 2. Still, the output is 0V. If you have any sample circuits for the LDO29300P2MTR, kindly help me solve the issues.

 

Then check your resistors & wiring.

Perhaps show a good, clear photograph of your setup.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
saran
Associate III

@Andrew Neil 

I have attached the images for your reference. Kindly let me know if I have made any mistakes

 

saran_0-1743219895566.png

WhatsApp Image 2025-03-29 at 9.11.29 AM.jpegWhatsApp Image 2025-03-29 at 9.23.29 AM.jpegWhatsApp Image 2025-03-29 at 9.27.10 AM.jpeg