2014-09-06 5:57 AM
Greetings,
I am doing a test series of stepper drivers with L6480 for furnace rotation control. There seems to be a problem with the device. The circuit is a copy of Eval 6480. SPI is up and functional, every register is correctly set. The problem is that L6480 cannot switch on all high-end transistors. The transistors I use are IRFB4310ZPBF (hexfet power mosfet, Vdss-100V, Ids -120 A, Rds-5mOhm, Qg-170nC) compared to the Eval 6480 (stripfet power mosfet, Vdss-100V, Ids - 25 A, Rds-35mOhm, Qg- 14nC) The device is running on 28 V DC, with Vboot-Vs=10,5 V, with GateConfig set to 96 mA / 3750 nS ( a total of over 330 nC). But even if the OCD is disabled it is unable to switch on the upper transistors. Could you help ? Thanks in advance! Eng. Tom Draganov , Alex Engineering Ltd. #l64802014-09-07 5:51 PM