cancel
Showing results for 
Search instead for 
Did you mean: 

L6474 Driver Stalling at 15kHz step frequency

smithderek2000
Associate III
Posted on August 05, 2014 at 00:06

Hello,

   We're having issues with the L6474PD driver and stalling. I'm testing it with the L6474PD evaluation board powered by 24V. Logic is at 3.3V. Motor runs fine below 15kHz, but right around that frequency it starts losing synchronicity and stalls out. How do we prevent this problem?

#stalling #l6474
1 REPLY 1
Enrico Poli
ST Employee
Posted on August 21, 2014 at 14:32

Hello Derek,

The maximum speed of a motor is usually limited by mechanics or supply voltage.

Try increasing the supply voltage of your system.

Regadrs

Enrico