2014-07-07 5:24 AM
I use the L6472 with step / direction inputs. Can I write to register 9 (TVAL_HOLD) at any time? I am polling the position counter to determine when the motor didn't move for a while. Then I switch from normal to standby current. Observation: sometimes during this transition the current regulation becomes unstable and OCD trips.
#l6472-current-regulation2014-07-13 1:55 PM
Maybe after it trips read the Tval register to see if noise spi affected the data you sent. I plan on doing the same thing, to set it to 50% standby current when the motor is stopped. Im using the L6474 and monitoring the step signal with the mpu.
How hot does your L6424 run ? Mine gets up to 75 deg C while holding at just 1.25 amps. When its spinning, it runs a bit cooler in the 50C range.