cancel
Showing results for 
Search instead for 
Did you mean: 

L6258 motor driver problems

puujakuori
Associate
Posted on September 08, 2005 at 03:36

L6258 motor driver problems

1 REPLY 1
puujakuori
Associate
Posted on May 17, 2011 at 10:18

I need help for controlling a L6258 motor driver. I have been drove it at the PIC micocontroller and it not to be able to work. If I leave all input lines on hight state motor will rotating very nice on itself (help with motor drive, not PIC). If I take phase lines along for example like full step mode , aren't they any effect on rotating. Microstepping mode doesn't work at all. So, is there any helping hand and give me for example for controlling this type motor driver ;)

[ This message was edited by: Jallu on 08-09-2005 07:09 ]