cancel
Showing results for 
Search instead for 
Did you mean: 

Can't find replacement IC

dpm2
Associate
Posted on November 19, 2007 at 10:20

Can't find replacement IC

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dpm2
Associate
Posted on May 17, 2011 at 10:18

HELP! I blasted the ST72F264G2B5 MC on my EvalPractiSPIN board.

I have looked all over the web for replacement chips but Noooo.

The only ones I have found is ST72F264G2B6 and I have to buy 480 of them; Yikes

.

I only need a hand full < 5 for replacements if this failure occurs again.

Does anyone know where I can get some of these chips?

Are these obsolete?

I'm located a few miles from the St Wherehouse in Phoenix if that helps.

Thanks: Dennis

andreasfiebich9
Associate II
Posted on May 17, 2011 at 10:18

Hello,

I was looking at www.newyorksemi.com - they seem to have some of it left !

Best regards,

Dipl.-Ing. Klaus Pelikan

mfederici2
Associate II
Posted on May 17, 2011 at 10:18

Hello Dennis. I'am your partner in this problem...like your.

now I 'm planning to re-produce the evalpractspin. I've only ST72264 mcu in SO version, but it's not a problem for me. Instead my problem is to have the FW, because the old MCU smoked for my error. So, I can reproduce the PCB craftmade using the SO MCU type but I haven't the FW. (from the ST's site it's possibile to update it only). do you think we can help ourself together? I can do two PCB and make a present of it for you. have you the FW or can you help me for this? contact me at

mailto:mfederici@rd-lab.it

;)

gaetano
Associate II
Posted on May 17, 2011 at 10:18

Hello,

after the installation process of EVALPRACTISPIN tool, in your root directory (tipically drive C:), inside ''Program Files/PractiSPIN'' folder there are three .s19 files (each one according to the motor type), that are the ST7's firmware binary files you are looking for.

I hope this helps you.

Best regards,

Tanio