L6229 L6235 +5V Supply
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-03 10:24 AM
Posted on December 03, 2014 at 19:24
For EVAL6229 or EVAL6235 with PractiSpin board it looks like 3.3V or 5V reference is from other PCB, is there a way for L6229 or L6235 to supply 5V (for EN, F/R, BRAKE) internally?
Does ST make compatible 8-52V to 5V (or 3.3V) DC-DC conveter that would be good companion for L6229 if this cannot make own 5V source (like L4971 but with fixed output and not needing so many external components?)
Labels:
- Labels:
-
Motor Control Hardware
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-15 7:07 AM
Posted on December 15, 2014 at 16:07
The EVAL boards can generate the 5V pull-up voltage through a zener diode.
For your final application ST proposes a wide range of step-down converters covering the 8V to 52V range. For example you can use thehttp://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63210
,http://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63207
andhttp://www.st.com/web/catalog/sense_power/FM142/CL1456/SC355/PF63205
.