2024-08-29 1:42 AM
I am using Simlis to carry out a simulation of AN5797 1KW bridgeless CCM-PFC pre-regulator based on the L4986A IC, I have built up the circuit, but it does not simulate and produces an error The voltage and currents of this circuit cannot be uniquely solved. I am unsure what is causing this error. The part is downloaded from ST. I have broken the design down by removing the L4986A and the positive & negative voltage sensing section that is driving VGS1-4 seems to give the expected gate control signals when GD is driven with a 68kHz square wave, but when the L4986A is added in it stops simulating, I have attached my simplis schematic. I have contacted Simplis and they are unable to find out what is wrong.
Do ST have .a functioning SIMPLIS schematic for the AN5797 bridgeless PFC shown in your application.
Look forward to hearing from you.
Regards
Ian
but the simulation fails to simulate.