2024-08-24 5:18 AM - last edited on 2024-08-25 10:59 AM by Tesla DeLorean
Hi ,
Could help me to identify the model of this TVs diode
it’s from WD external 4TB HDD
Thanks in advance.
2024-08-24 6:17 AM
"the marking is SUA, which corresponds to the SMA6F5.0A-TR, which can be found today with 6AI marking."
2024-08-24 6:26 AM
Thanks for reply ,
What about the first TVs Diode which stands with SUG marking ?
2024-08-24 8:54 AM
"SUG stands for the SMA6F13A-TR"
https://community.st.com/t5/power-management/unable-to-find-diode-or-cross-ref/td-p/683783
2024-08-24 3:41 PM
@Lina_DABASINSKAITE , here's another example of missing labels. The forum sees a slow but steady stream of such chip identification help requests, but there's no forum label for it. In lieu of a dedicated subforum, a dedicated label would be nice.
2024-08-25 3:59 AM - edited 2024-08-25 3:59 AM
@BarryWhit There is a label: Power Managment > Discretes
Well, maybe not the ideal combination, but should mostly work - doesn’t it?
Regards
/Peter
2024-08-25 10:57 AM - edited 2024-08-25 12:30 PM
As it is it shows up in my feed, I'm Ok with it, and the more times we answer the better the chance of a direct Google Hit for the self-service customers
These particular diodes being a pain due to lack of marking documentation, and the markings changing from current issue parts.
ST STMICRO DIODE SUA SUG MARK MARKING
HARD DRIVE DIODES
600W TVS
OLD: SUA SMA6F5.0A NEW: 6AI
OLD: SUG SMA6F13A NEW: 6AY
2024-08-25 11:45 PM
Yes, this may be a little confusing, but all SMA6F (package SMA Flat) are obsolete and no longer visible on the ST website, please do not confuse it with SMA6J (package SMA).