cancel
Showing results for 
Search instead for 
Did you mean: 

Issues with VNQ9080AJTR Quad-Channel high-side driver Output and Input Behavior.

Divyansh12
Associate

Hello STM Community,

I'm currently working with the VNQ9080AJTR Quad Channel High-Side Driver, and I'm encountering a couple of issues that I hope someone here can help me resolve

1.Output Voltage Regulation: With a constant VCC supply of 12V, the output of the IC is randomly regulated to 7-8V instead of maintaining a stable 12V output. This issue seems to occur intermittently, and I can't pinpoint a specific trigger for when it happens. Has anyone experienced similar behavior? What could be causing the output voltage to drop unexpectedly?

2.Input Pin Voltage: I have connected the input pin (which is supposed to take signals from the microcontroller) to control the driver, but at times, I'm reading 7-8V at this input pin instead of the expected logic-level voltage.

For both issues, I’ve verified my connections and ensured proper grounding. The behavior is random, making troubleshooting difficult.

Datasheet : https://www.st.com/resource/en/datasheet/vnq9080aj.pdf

1 REPLY 1
MBONA.1
ST Employee
Dear Divyansh12,
 
 there is something strange on this behavior.
 
To support you we need to have a schematic and more information.
 
Waiting for your feedback.
 
BR