cancel
Showing results for 
Search instead for 
Did you mean: 

Is the STEVAL-CTM009V1 (L6491) capable to drive a stepper motor?

NBOUM.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Well, the STEVAL-CTM009V1 implements a three-phase driver with 5kW power, so it has three half-bridges, whereas a stepper motor typically requires two full bridges, i.e. four half-bridges.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Well, the STEVAL-CTM009V1 implements a three-phase driver with 5kW power, so it has three half-bridges, whereas a stepper motor typically requires two full bridges, i.e. four half-bridges.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.