2025-01-20 05:41 AM
I'm using a single L9963E and it works fine. However, I couldn't start daisy chain connection. When I consider BMS architectures in datasheet, all of them has L9963T transceiver to communicate with further IC. My custom PCB doesn't provide L9963T.
So I have two question:
1- Do I really need a transceiver for USE MULTİPLE l9963E slaves ?
2- Can I use the transceiver on EVAL-L9963E-MCU for this purpoeses?
Bear in mind, I'm using an external MCU, not built in SPC MCU chip.
Lastly, as I said, I can succesfully communicate single IC and I'm using a cable that has low capacitance.