2020-04-28 10:38 PM
Hi,
I've connected a IHM02A1 expansion to drive two stepper motor on a Nucleo-F302R8. I've followed the user manual UM1964 to setting up the example both in the standalone version and in the UART version. I can't achieve to have the motors move and I have all the time the red led on the IHM02A1 (connected to the L6470 FLAG signal) . I've check in the community and I've seen that somebody else has faced the same problem but I'm not able to find the way to solution it.
What could I try to do to check where is the problem?
Thanks in advance for any suggestion
2020-04-29 7:31 AM
SOLVED
I add some information. Hope it helps!
The problem was in the SPI pins and I want add something that could be helpful for who has a problem like this.
There is a problem in the X-NUCLEO-IHM02A1 documentation:
In the documentation (UM1964-User manual-DocID028481-Rev 1- pag. 15/24):
SB10 >> PB15 as L6470_1_SDI
SB26 >> PA7 as L6470_1_SDI
SB32 >> PA6 as L6470_0_SD0
SB11 >> PB14 as L6470_0_SD0
SB34 >> PB3 as L64701_SCK/L64702_SCK
SB12 >> PA5 as L64701_SCK/L64702_SCK
SB13 >> PB13 as L64701_SCK/L64702_SCK
The real connection is:
SB10 >> PA7 as L6470_1_SDI
SB26 >> PB15 as L6470_1_SDI
SB32 >> PB14 as L6470_0_SD0
SB11 >> PA6 as L6470_0_SD0
SB34 >> PB3 as L64701_SCK/L64702_SCK
SB12 >> PB13 as L64701_SCK/L64702_SCK
SB13 >> PA5 as L64701_SCK/L64702_SCK
The example X-CUBE-SPN2 set SPI2 at this pins:
/**SPI2 GPIO Configuration
PB13 ------> SPI2_SCK
PB14 ------> SPI2_MISO
PB15 ------> SPI2_MOSI
So I finally use SB26, SB32, SB12 and everything works.
Francesco
2020-04-29 9:12 AM
How did you configure the device?
A wrong setup of the configuration parameters of the voltage mode driving could cause several issues.
For more details could you refer to AN4144: Voltage mode control operation and parameter optimization
Moreover, what sequence of commands did you use to move the motors?
Ffor more details, refer to the L6470 application Note: L6470 Resources
2020-04-29 10:16 PM
Hi @Cristiana SCARAMEL , thanks for your reply. I'll read with attention the AN suggested about the voltage mode driving.
About the original issue I solved the problem reviewing the SPI pins.
I would like signal you the schematic error in the X-NUCLEO-IHM02A1 documentation (UM1964-User manual-DocID028481-Rev 1- pag. 15/24 https://www.st.com/resource/en/user_manual/dm00237629-getting-started-with-xnucleoihm02a1-twoaxis-stepper-motor-driver-expansion-board-based-on-l6470-for-stm32-nucleo-stmicroelectronics.pdf) about the SPI pins (details int the first reply at this post).
Many thanks for your interest and your kind reply.
Francesco