cancel
Showing results for 
Search instead for 
Did you mean: 

how to collect the parameters of the motor (the speed at which the motor is running, the current flowing in the motor) using steval esc001v1. Thanks in advance.

Vmudu
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

For better support please visit the page "Drone zone". To monitor all the motor parameters you need to open the GUI of the ST Workbench tool and connect the PC with UART dongle.

BR

Giuseppe