cancel
Showing results for 
Search instead for 
Did you mean: 

How to Avoid OverCurrent Error using STSW-SPIN3204 Library ?

ASing.41
Associate
  • I am using STEVAL-SPIN3204 development Board & using STM motor Library STSW-SPIN3204 .I am using a Maxon Motor with 12V DC input voltage.
  • I am successfully able to run motor at 14k RPM but when I try to run motor at 25K RPM , my motor stalls & hits over-current error . I shouldn't be hitting this error as Motor is only drawing 0.4 Amps at this time.
  • How can I avoid this error and stop my motor from Stalling ?

Any help in this matter will be really helpful .

Regards & Thank you.

0 REPLIES 0