2014-10-30 01:36 AM
hello:
Air condition out fan motor is roating because of wind . I start up the motor will appear start up failed. How can I do?2014-12-12 02:48 AM
Ciao
We call this feature: ''Startup on the fly'' and untill now has been provided only under request. We plan to have it as official feature of the next release planned for Q1 '15. Ciao Gigi2015-03-13 02:11 AM
good to hear, I also recognized this and am now eagerly waiting for the update :)
Regards Frank2015-03-13 02:12 AM
Question: will this require board changes like measuring phase voltages via ADC, or have you found a pure software based solution? When thinking about this, it seems difficulty to me. For example, which initial phase voltages to set when enabling the power stage...
Regards Frank