2022-04-29 10:49 AM
Good day
I am currently designing a BLDC driver, with the L6235D chip, ideally I wanted to use the L6235PD but there isn't any stock available.
So basically I am concerned that the L6235D will not be able to drive my motor, the motor requires at least 1.5A, based on my thermal calculations it would seem like the L6235D would be running at a very marginal point. Is there anything I can do to reduce the thermal coefficient?
Kind regards
Yuveer
2022-05-04 06:17 AM
Hello @Na.1 and welcome to the ST Community.
I can only suggest to use an heatsink with a thermal interface material.
Take into account, however, that with this type of package the benefits are negligible.
2022-05-04 07:41 AM
2022-05-05 02:18 AM
Hi @Na.1,
I edited the previous post because I would not want to pass the message that heatsink can be resolving.
Also the effect of the thermal interface material to the bottom of the chip (or between the top and heatsink) can be negligible.
The main role of thermal dissipation in SO package are to the leads.