2018-08-03 02:04 AM
Hi,
Greetings!
We are in the process of finalizing 230 Watts load Phase Dimmer Schematic wherein we need some help on below points.
Please find attached copy of Phase Dimmer Schematic for your reference
1. What should be value of “INDUCTOR�? considering LINE SUPPLY to be
1a. 230VAC to 250VAC, 50-60Hz
1b. 110VAC to 130VAC, 50-60Hz
2. Make and specifications of Inductor
2a. 230VAC to 250VAC, 50-60Hz
2b. 110VAC to 130VAC, 50-60Hz
3. Are Snubber component values correct?
3a. 230VAC to 250VAC, 50-60Hz
3b. 110VAC to 130VAC, 50-60Hz
4. Can we use resettable fuse for short circuit protection? What should be the specifications?
4a. 230VAC to 250VAC, 50-60Hz
4b. 110VAC to 130VAC, 50-60Hz
5. Any protection needed to avoid short circuit failure of Triac?
Regards,
Dinesh