2025-01-07 3:43 AM - last edited on 2025-01-07 4:27 AM by Andrew Neil
Moved from Feedback forum.
I am exploring the possibility of using the EVAL6498L Evaluation Board to reverse the polarity of a DC bias in my circuit, and I would like to confirm whether it suits my application.
I would greatly appreciate any technical documentation, user guides, or application notes relevant to this use case. Please let me know if you need additional details about my setup or application.
Thank you for your support. I look forward to your response.
Best regards,
Arun
2025-01-07 6:09 AM
Welcome @arunrhpd88, to the community!
I'm afraid that you won't be able to use the board for this. In order to be able to make a suggestion as to how you can realise this as an alternative, you should provide details about the GDD load in addition to the level of the voltage to be reversed, e.g. switching frequency, time sequences of the switching operations or the required current of the GDD.
Regards
/Peter
2025-01-07 6:22 AM
Thank you for your prompt response and for considering my inquiry. I appreciate your guidance and would like to provide the additional details requested regarding my application:
2025-01-07 7:50 AM
I don't think it'd work. Since L6498 has charge-pump circuitry to power up high-side driver, there is undocumented minimum switching frequency to generate enough power, to keep driver in "operational state".
It 'd be easier to build switching polarity circuits using solid state relays, like
https://standexelectronics.com/wp-content/uploads/datasheets/55/5521308110e.pdf
2025-01-07 8:02 AM
The idea with the SSR is very good, alternatively you could also build a discrete full bridge. However, the effort with P-channel MOSFETs on the high-side and N-channel MOSFETs on the low-side (each at least 150V capable) is greater than with the SSRs mentioned by @MasterT, especially as you also have to control and protect the gates.