2011-01-31 12:15 AM
EVAL6470 operation via SPI
#l6470 #l6470 #l6470 #l6470 #l64702011-05-17 01:20 AM
Dear Mr.,
I confirm the STEVAL-PCC009V1/V2 drivers are not compatible with Windows 7 64-bit.
At the moment we have not a scheduling of a new driver release.
Best Regards
Enrico Poli
2011-05-17 01:20 AM
Any update on this information? I note that the dSPIN is not compatible with Win7 64-bit. Will this be addressed?
2011-07-07 11:38 PM
Dear all, after i tried any methods to drive EVAL6470,
it can move,run..., but it cannot read/write registers.
do anyone know where is the problem??
Best regard, Omar
2011-07-10 06:53 PM
Registers can read/write well now!!!
I forget to clear data after writing a read command.
Best Regards,
Omar