Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STL62P3LLH6 Safe Operating Area correct?

Posted on March 31, 2016 at 15:28I'd like to know if the STL62P3LLH6 P-channel MOSFET's Safe Operating Area chart is correct in http://www.st.com/web/en/resource/technical/document/datasheet/DM00105886.pdfhttp://www.st.com/web/en/resource/technical/...

Major Mistake in my design

Posted on March 29, 2016 at 12:45Hi, I attached my schematic to help in my discussion.  I made a huge mistake by selecting a Linear Regulator U200: (12Vin - 5Vout).  Roughly I'm drawing about 1.5Amps, therefore my power dissipated across the IC is (...

BC1999 by Associate II
  • 853 Views
  • 0 replies
  • 0 kudos

ST1CC40 no load output voltage

Posted on March 08, 2016 at 05:48Hi, I'm trying to build a constant current LED driver using the ST1CC40. I built a prototype version and noticed that with no load attached, the entire Vin (in my case its 12V) is seen at the output. Is this normal? ...

L4984D

Posted on March 28, 2016 at 07:43Hello! I want to ask a question about chip PFC L4984D.1. Calculate the inductor according to datasheet. When the input voltage is greater than 200 volts, the inductor begins to make noise, heavily distorted input cur...

Using multiple L6472 ICs on same circuit board

Posted on March 25, 2016 at 14:04I am working on an application where I need to use three L6472 ICs on the same board. I am wondering what external components can be shared between 2 or 3 L6472's. For example, can one cap elec 100uf 63V on the VS in...

Bug in EVAL6480H-DISC document

Posted on January 18, 2016 at 13:21I think there is a mistake in the scheme: Checking data sheet (and a board built by myself), the red line (2) is wrong, and it is necessary the blue line (1). I have destroyed 3 L6482 chips before to find out what ...

0690X00000605dDQAQ.png 0690X00000605aiQAA.png
val_ltd by Associate II
  • 1051 Views
  • 1 replies
  • 0 kudos

L9942 Set Up

Posted on March 18, 2016 at 20:15In the datasheet, Register 0 has 5 bits (P0-P4) that are defined as ''This bits control position of motor, e.g. 00000 step angle is 0, 01111 step angle is 180.  There is no table which defines how to derive the other...

BLDC commutation with hall sensors

Posted on May 30, 2014 at 17:09The original post was too long to process during our migration. Please click on the attachment to read the original post.

ssatjas9 by Associate
  • 1648 Views
  • 1 replies
  • 0 kudos

L6470H does't switch between SYNC and BUSY mode

Posted on March 12, 2016 at 19:10 Hello. I use L6470H chip. I found a issue of the chip. I want switch mode BUSY and SYNC in my program to control of the step clocking. I can write ''1'' to SYNC_EN bit of the STEP_MODE register. BUT I ca...