Driving a proportialnal hydraulic valve with VN5E050?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-08-06 2:43 AM
Posted on August 06, 2014 at 11:43
Hello
I would like to control a hydraulic valve (24V, 0-2.6A) proportional (0-100%) with a PWM signal from a MCU. I need to measure the current, detect open loop and short detection to VCC. I found the VN5E050J-E, but I'm not sure it can handle PWM as the datasheet says nothing about maximum switching frequency. Would 20 kHz PWM be ok? Is there a better choice than VN5E050 for driving a proportional hydraulic valve (24V, 0-2.6A)? Maybe there is an IC with a h-bridge solution to eliminate power loss of the diode? Any suggestions are appreciated! Henrik
Labels:
- Labels:
-
Motor Control Hardware
0 REPLIES 0