2024-05-29 05:46 AM - last edited on 2024-05-29 05:56 AM by Peter BENSCH
could you help me to know why the dimension differnet in 2 datasheets while the supplier package is SOT-23 with pincount 3 pins
> the dimension for first diagram is ( Length = 3.04(Max) - Width = 1.75(Max) - Height = 1.3(Max) )
> the dimension for second diagram is ( Length = 2.9 - Width = 1.3 - Height = 0.95 )
i think the 2 parts should have the same dimension because it have same package and pincount .
why there are tolerance in dimension and not unified for same pincount and supplier package .
Thanks
2024-05-29 07:33 AM
The two devices you mentioned come from completely different divisions: the first is an automotive Schottky BAT54-Y, the other an industrial shunt reference LM4040. Only the pin spacing is standardised for SOT23-3L, the package dimensions can differ slightly depending on the manufacturing machine currently used. The respective data sheet is always decisive.
Hope that helps?
Regards
/Peter