Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-A6986IV3 grounding capacitors

Hello, I am strongly considering using the STEVAL-A6986IV3 based design for a 4 channel isolated gate driver power supply.  One thing that looked strange in the the schematic was the four ground capacitors Cgnd1,2,3,4 which are 4.7nF 2000V rated. The...

jwiseman by Associate
  • 785 Views
  • 1 replies
  • 1 kudos

Resolved! Questions about to Auxiliary power supply with VIPER06

HiI have a question about the conection of VIPER06 module as auxiliary power supply.  I Have a power stage PFC with L6562  and two capacitor in series as outuput capacitor. Then, i need a 15V aux power supply. Can i connect the VIPER06 Flyback stage,...

mcolin_0-1744305849952.png
mcolin by Associate
  • 817 Views
  • 1 replies
  • 1 kudos

Resolved! L6982C33DR & L6982C50DR always provide 2.5V output

Dear Community,I’m currently testing the L6982C33DR and L6982C50DR to supply 3.3V and 5V to my board.I followed the reference design provided in the user manual and completed the PCB layout accordingly.However, when I power the board with 12V (Power+...

Screenshot 2025-04-08 at 23.39.02.png Screenshot 2025-04-08 at 23.39.26.png
Sheng123 by Associate II
  • 1278 Views
  • 3 replies
  • 0 kudos

l6235 brake issue

i have a design using the L6235 motor controller. when the motor is running at 4800 I applied the brake and disabled the enable pin of the IC, all worked fine, But i was getting the motor overrun because of the inertia of the gears.I tried to applied...

Resolved! STEVAL-IPM10B Evaluation Board Purpose of "PWM_Vref" Pin

Hello again, dear STMicroelectronics team,While reviewing the schematic sheets of the STEVAL-IPM10B Evaluation Board, I came across a connector pin labeled 'PWM_Vref' (highlighted with a green circle in the image below). However, I couldn't find this...

Hasan06_0-1744094667017.png
Hasan06 by Associate II
  • 1115 Views
  • 2 replies
  • 1 kudos

Resolved! STGIB10CH60TS-L Isolation Issue

Hello, would it cause any issues if 'PWR_GND' (highlighted in green) and 'SGN_GND' (highlighted in pink) are not referenced to the same ground?Thank you in advance. Best regards.

Hasan06_0-1744009471564.png
Hasan06 by Associate II
  • 1041 Views
  • 2 replies
  • 1 kudos

T1610T-8i won't turn off above 60c, should work to 100c

I apply three phases at 115vac, 400hz.I apply a 10A load. I turn on the Opto-Triac (VOT8121AB), and current runs thru the Triac under test(TUT) (T1610T-8i) and ac voltage appears at the output (ex; see CSSI_R_PhaA_Out, loc=A5, of Attached schematic “...

Burtb6 by Associate II
  • 1973 Views
  • 2 replies
  • 0 kudos

Resolved! STEVAL-WBC86TX and STEVAL-WLC38RX coil change

Hello everyone,I got the above mentioned Eval boards with the following adaptions to suit my application:- Tx coil connected to STEVAL-WBC86TX: WE 760308101104 - Rx coil  connected to STEVAL-WLC38RX: Custom PCB antenna with ~1.5 µH self-inductance, ~...

David101_0-1743587332564.png David101_1-1743587741000.png
David101 by Associate
  • 1685 Views
  • 3 replies
  • 1 kudos

Resolved! E fuse with ASIL B compliance

Is VNF1048FTR of ASIL B compliance? If not can you suggest any E fuse with ASIL B compliance with 48V system, with SPI, current sense

Anjana1 by Associate
  • 867 Views
  • 1 replies
  • 0 kudos

Resolved! HVLED007

Hello, Good Morning Can i design SMPS using HVLED007 which should work on universal input and should provide 24v 2amp at its output it is PFC too. The most challenging part is to calculate and wind flyback transformer. I've some transformer bobbins a...

D_N by Associate II
  • 877 Views
  • 1 replies
  • 2 kudos