cancel
Showing results for 
Search instead for 
Did you mean: 

Control Voltage with Phase current control

fedex03
Associate II
Posted on July 17, 2013 at 23:38

Hi Everybody,

I use

the

integrated

L6470

to control

a stepper motor

with

the following characteristics:

Step angle

1.8

Holding Torque

0.06Nm

Rated current

0.67

A

Rod diameter

5mm

Frame size

28 x

28mm

Rod length

18mm

Permanent magnet

stepper motor

,

hybrid

Number of

wires

4

Resistance

5.6?

per phase

Rated voltage

3.8 V

The

integrated

L6470

is powered

at 12V

but I

would like to make

sure that

the motor voltage

is

3.8V

.

I saw on the

datasheet

that I can adjust

the motor voltage

with

the

Phase

current control

.

Unfortunately

I didn't

have

clear about the

parameters

of the equations

to derive

the value

Kval

.

Can anyone explain

me how to get the

value

Kval

?

The motor

is controlled with a 

microcontroller

STM32F103

via

SPI

.

I communicate

the

parameters

KVAL_RUN

,

KVAL_ACC

,

KVAL_DEC

with SPI.

Thanks a lot

Bye

#stepper-motor-driver #l6470
0 REPLIES 0