cancel
Showing results for 
Search instead for 
Did you mean: 

CMC for PM8805. Do I need it?

SIlia.1
Associate II

At the datasheet at figure 7 you use CMC befor connecting it to DC2DC.

I connect the PM8805 to DC2DC LTM8027.

If I don't put the CMC will it be worng?

BR

Shmuel

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Figure 7 of the data sheet is only a simplified circuit to illustrate the principle. Further information can be found in the design tip DT0149.

There is no generally applicable recommendation for the common mode filter because its dimensioning depends on factors such as the type of SMPS or PoE class.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

Welcome, @SIlia.1​, to the community!

the data sheet of the PM8805 writes about the necessity of a common mode filter in section 4.9:

In most of the PoE applications a common mode filter is required to allow the PoE converter to be compliant with the applicable EMI standards. The right position where such a filter is introduced is between PM8805 and the PoE converter, as shown in Figure 7.

Not using a common mode filter cannot therefore be said to be "wrong", but you should ensure that you comply with EMI regulations.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SIlia.1
Associate II

Hi Peter,

Thanks for the fast respond.

The answer is very clear.

At the same figure there are 2 CMC.

Which one is prefered? the t? or the L? Do you have a prefered part number?

BR

Shmuel

Peter BENSCH
ST Employee

Figure 7 of the data sheet is only a simplified circuit to illustrate the principle. Further information can be found in the design tip DT0149.

There is no generally applicable recommendation for the common mode filter because its dimensioning depends on factors such as the type of SMPS or PoE class.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SIlia.1
Associate II

Thanks a lot

Peter BENSCH
ST Employee

You're welcome!

If the problem is resolved, please mark this topic as answered by selecting Select as best under your preferred answer. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.