2024-03-08 4:47 AM - last edited on 2024-03-08 5:08 AM by Peter BENSCH
The datasheet suggest its suitable for SMPS / lighting power supplies. Not clear if they can be used for the inductive load at the output of the hotswap controller.
Solved! Go to Solution.
2024-03-08 6:03 AM
The DC fan then draws approx. 6A, so that the freewheeling diode must also be able to withstand at least this current, which is why a diode with higher current is recommended, e.g. the STPS10H100C.
Theoretically, you can also use a TVS, but with a 340W motor it is a challenge to find a suitable one. However, TVS in a suitable power class are typically significantly more expensive than a freewheeling diode as mentioned above.
It is also a question of the desired behaviour: with a freewheeling diode, the motor continues to run at falling speed, while the TVS limits the voltage and thus slows the motor down more.
Regards
/Peter
2024-03-08 5:05 AM
Welcome @vineeth_1511, to the community!
The STPS2H100 is extremely fast when switching due to the Schottky operating principle, so that you can use it for freewheeling a coil under certain conditions:
Hope it helps?
Regards
/Peter
2024-03-08 5:39 AM
The thing is we are using the DIODE as freewheeling for DC fan powered at 54V which consumes around 340W. Is it better to use this Diode or a TVS diode in the scenario? or Do we need to have a diode with higher rated current?
more over the Hotswap IC is rated 80V max so is it okay to use a diode with 100V or should we go for lower value?
2024-03-08 6:03 AM
The DC fan then draws approx. 6A, so that the freewheeling diode must also be able to withstand at least this current, which is why a diode with higher current is recommended, e.g. the STPS10H100C.
Theoretically, you can also use a TVS, but with a 340W motor it is a challenge to find a suitable one. However, TVS in a suitable power class are typically significantly more expensive than a freewheeling diode as mentioned above.
It is also a question of the desired behaviour: with a freewheeling diode, the motor continues to run at falling speed, while the TVS limits the voltage and thus slows the motor down more.
Regards
/Peter