The datasheet suggest its suitable for SMPS / lighting power supplies. Not clear if they can be used for the inductive load at the output of the hotswap controller.
The thing is we are using the DIODE as freewheeling for DC fan powered at 54V which consumes around 340W. Is it better to use this Diode or a TVS diode in the scenario? or Do we need to have a diode with higher rated current?more over the Hotswap IC ...