2019-04-09 9:39 AM
Hello,
I appears that STD25N10 is designed to a replacement for the STD15NF10. Do you confirm?
Do you have any comparisons or recommendations about external gate resistors when this device is used in a three phase inverter application?
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.
Solved! Go to Solution.
2019-04-09 9:40 AM
STD25N10F7 can be suitable replacement for the legacy part STD15NF10, due to it's superior Rdson and similar current rating. The F7 technology is a trench style MOSFET v. the NF planar style, so it will switch faster and may have weaker thermal, avalanche, and SOA characteristics. A close comparison by datasheet is necessary to determine if it is suitable for your application.
Gate resistor selection is highly dependent on application considerations - Layout, switching frequency, EMI constraints, current, etc. We recommend laying out for both turn on and turn off resistors and adjusting them by experiment to meet your needs.
2019-04-09 9:40 AM
STD25N10F7 can be suitable replacement for the legacy part STD15NF10, due to it's superior Rdson and similar current rating. The F7 technology is a trench style MOSFET v. the NF planar style, so it will switch faster and may have weaker thermal, avalanche, and SOA characteristics. A close comparison by datasheet is necessary to determine if it is suitable for your application.
Gate resistor selection is highly dependent on application considerations - Layout, switching frequency, EMI constraints, current, etc. We recommend laying out for both turn on and turn off resistors and adjusting them by experiment to meet your needs.