2018-05-24 12:31 AM
Dear All,
I have been working on a project where I need to Switch on Two devices using Two BTA06 controlled by Digitally Opto-Triac. Line and Neutral are same for both.
Attached is the schematic.
I have issue that when I swithch ON Triac 1 and keep Triac 2 OFF still I get 120V output on triac2 which should be zero.
However, switching OFF Triac 1 voltage is gone.
Can you please suggest what could I have missed?#bta06-triac